STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

D flip-flop

Hi,I need to normalize the asynchronous transmission to a specific baudrate in real time. I know flip-flop D is fine, but I don't want to add extra elements to the layout. Can I do it with timers or maybe some other solution?

PKurz.1 by Associate III
  • 2081 Views
  • 3 replies
  • 0 kudos

STM32F429 Sleep mode and Systick

Hi'I'm using an STM32F429 in a project that needs to enter to sleep mode.I can't determine if I need to disable manually the HAL tick previously to entering in sleep mode, or if the sleep mode enter instruction does it by itself. Can anyone tell me?T...

How to send a remote data request in CAN-FD

Hello,I am working on CAN-FD project and and I am able transmit and receive data. Currently it is continuously sending and receiving the data. But I want to send data only when receiver sends data requests. How can I do that? thanks for help

Resolved! How to properly initialize shared arrays on STM32745?

In my application I am using initialized data in shared memory for the use in a user interface. The memory is in the SRAM2 at 0x30020000. Both cores need to access that data, so I use code of the following form:__attribute__((section(".sram2"))) uiSe...

Hansel by Senior
  • 4072 Views
  • 6 replies
  • 0 kudos

Resolved! My kingdom for some samples! (STM32L4 + LQFP48 + DFSDM)

Yes, I have tried contacting the local ST sales reps here in Australia - no response.Sorry, I've resisted asking this question for a fair while because I know many have greater need. But I thought I would ask this question just in case there is a sec...

gregstm by Senior III
  • 5424 Views
  • 12 replies
  • 1 kudos

Resolved! I'm currently integrating a Micron MT29F1G01ABAFDWB NAND flash with a STM32L4R5ZIT using its OctoSPI peripheral. According to Table 119 on page 556 of the SMT32l4+ reference manual RM0432, Micron mode is not supported. Which OSPI modes does this include?

I'm currently trying to integrate a Micron MT29F1G01ABAFDWB NAND flash with a STM32L4R5ZIT using its OctoSPI peripheral. A colleague of mine found Table 119 on page 556 of the SMT32l4+ reference manual RM0432 that seems to indicate that our MCU does ...

AHart.3 by Associate
  • 2608 Views
  • 3 replies
  • 0 kudos

How to start STM32F767ZI Nucleo board when connected to an external 5 VDC power supply ? I set JP3 to E5V, when I switch on the 5 VDC external power, green led LD6 PWR goes on but I have to press the reset button B2 to start the program running.

Not clear if I have to remove SB111 (only if powered with 3.3 VDC according manual)So, how to make the board running its program without user intervention when it is powered via E5V (pin 6 and 8 of CN11)Thank you, J.

jea74 by Associate III
  • 1064 Views
  • 1 replies
  • 0 kudos

Auto baudrate detection STM32G0 - Error calculation

Hello,I consulted :https://www.st.com/content/st_com/en/search.html#q=usart%20stm32G0-t=products-page=1I was wondering where to find an AN describing "Error Calculation" for STM32G0Or if the below document (AN4908) is globally applicable for every pr...

Sego2 by Associate III
  • 1123 Views
  • 1 replies
  • 1 kudos