cancel
Showing results for 
Search instead for 
Did you mean: 

How to switch GPIO PORT's individual pin into analog input mode without disabling whole GPIO port before going into Stop mode, how to do it?

Shilpashree Madhu
Associate III
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
waclawek.jan
Super User

For example, to set PA5 to analog mode:

GPIOA_MODER |= (3 << (5 * 2));

where 3 is 0b11 for Analog Mode as given by GPIOx_MODER description in the GPIO chapter of RM; 5 is for PA5; 2 is because there are 2 bits per pin in GPIOx_MODER.

JW

View solution in original post

8 REPLIES 8
TDK
Super User

Please include your chip number in posts.

Set the appropriate bits within GPIOx->MODER to analog mode.

If you feel a post has answered your question, please click "Accept as Solution".

The chip I'm using is STM32L4R5ZI-P.

My question is what if I want to switch only a particular bit ​to Analog mode without switching whole GPIO PORT into Analog mode before entering to Stop2mode..

> My question is what if I want to switch only a particular bit ​to Analog mode without switching whole GPIO PORT into Analog mode before entering to Stop2mode..

Yes, that is the question I answered.

Set the bits associated with that pin to analog mode and leave the bits associated with other pins unmodified.

You can also use HAL_GPIO_Init to do this.

If you feel a post has answered your question, please click "Accept as Solution".

Thanks for your response @TDK​ 

Bit set is quite confusing,

Can you please help me with that?​

waclawek.jan
Super User

For example, to set PA5 to analog mode:

GPIOA_MODER |= (3 << (5 * 2));

where 3 is 0b11 for Analog Mode as given by GPIOx_MODER description in the GPIO chapter of RM; 5 is for PA5; 2 is because there are 2 bits per pin in GPIOx_MODER.

JW

TDK
Super User

If you're not comfortable with register-level manipulation, I would suggest sticking with HAL.

To change PA5 to analog mode:

    GPIO_InitTypeDef GPIO_InitStruct = {0};
    GPIO_InitStruct.Pin = GPIO_PIN_5;
    GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
    HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

If you feel a post has answered your question, please click "Accept as Solution".

Thank you soo much @TDK​ (ST Employee)​ 

Your explanation was very informative.

Much appreciated for the explanation, Thank you very much@waclawek.jan