STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Uart3 in stm32f103c8 not working

hi,i am trying uart with dma in stm32f103c8 with uart3 after n try i found that uart3 in stm32f103c8 is not working then in polling I observed that the TX pin is not getting high and low so I toggle that pin it toggles as a digital pin so I think t...

ABhat.7 by Associate III
  • 5928 Views
  • 12 replies
  • 0 kudos

why can't I change the clock

I inherited someone else's code who knows more about the STM32L1 architecture than I. In some code paths, the HSI can get changed to 8Mhz from the HSE of 32Mhz, and sometimes it can't.It fails because of this loop timing out.do { HSIStatus = RCC->C...

DBecc.1 by Associate II
  • 2256 Views
  • 6 replies
  • 0 kudos

I need help with I2C between a Arduino board and a STM32F103

I have been trying to make the Arduino talk to the STM32 via I2C but i just cant get it to work. The STM has to be in a form of a slave mode but i can't seem to figure it out. So if there is anyone who could help me or give me a form of an example fr...

NNams.1 by Associate
  • 1225 Views
  • 2 replies
  • 0 kudos

Questions about current injection on STM32G431CBT3 pins.

Hello, i have some questions about current injection onSTM32G431CBT3 pins.On datasheet Table 15 it is reported:IINJ(PIN) -> Injected current on FT_***, TT_xx, NRST pins ->-5/0NOTE3:Positive injection (when VIN > VDD) is not possible on these I/Os and...

ABido.1 by Associate II
  • 5573 Views
  • 5 replies
  • 0 kudos

Resolved! STM32F767 SPI slave weird behaviour

Dear community, I am facing a weird problem on using the SPI after migrating my codes from STM32F407 to STM32F767.The SPI is configured as slave and interfaces with another STM32F406 MCU as master. The data received by the slave is sometimes shifted ...

STM32F746G stucks in TIM6_DAC_IRQHandler?

Hello, everytime when I try to debug my program it stucks after the HAL_Init() in the main, so it never actually reaches the code provided by me. As I stepped through the code, I noticed that it gets into a infinite loop where it always calls a funct...

XFlas.1 by Associate
  • 5066 Views
  • 8 replies
  • 2 kudos