How to change flash start address without linker file
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-12-31 3:18 AM
I need to change my flash jump address when I update firmware. I am using sm32h750 microcontroller, I can change the application code start address with flash .ld (linker) file with this
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 192K
CCMRAM (rw) : ORIGIN = 0x10000000, LENGTH = 64K
FLASH (rx) : ORIGIN = 0x8100000, LENGTH = 64K
}
But I dont want to change anything on this file, I want to change only `FLASH register boot address FLASH_BOOT_CURR)` If I dont change .Ld file and configure these registers to what I want to start. Is program starts this address or not ?
I need this way because of the keep the last code on flash. If I change the flash start address so I can control the where can I copy.
If I change the flash registers at the time of init, will it be enough on its own to start from that address?
- Labels:
-
STM32H7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-12-31 6:40 AM
STM32H750 has 128KB of flash at 0x08000000 to 0x0801FFFF in one bank.
Only Chuck Norris could change the boot address of STM32H750 to 0x8100000 but he is retired long ago.