STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Observing the different execution time for a function if placed at different code memory location on STM32F765NIHx controller

e.g: Below are the execution time of memset() function at different locations.1. memset() plcaed at 0x0000000000219e96 : Time = 57.10 usec for 3k buffer size.2. memset() placed at 0x0000000000219d42 : Time = 28.66 usec for 3k buffer size.- memset is ...

AN.4 by Associate II
  • 879 Views
  • 0 replies
  • 0 kudos

RTC criteria for activating CSS

Hi ST Community.A colleague and I were having issues on an STM32L4, in that the CSS detects an LSE failure and swaps to the LSI.We looked at Errata ES00335 - Rev 15 and it confirms what we see that the LSI becomes unstable. We're looking for a workar...

AFahr.1 by Associate III
  • 2547 Views
  • 3 replies
  • 0 kudos

Synchronization of timers in stm32f7

Hi Sir / Madam,I am trying to synchronize two timers or reduce delay between two timer outputs.Yellow signal represents low frequency signal ( Timer 3 around 4Khz ) and blue signal represents high frequency signal ( Timer 1 around 1.5Mhz ). They are ...

0693W00000NrwMSQAZ.png
svLag by Associate II
  • 2188 Views
  • 3 replies
  • 0 kudos

Resolved! Can't communicate with another device via UART

I've been fighting this problem for some time. I have a simple custom made board based on STM32G05. I'm utilizing 2 UARTs. One of them I use just for serial port debug. Takes keyboard input (but don't use it) and print out data for debugging. The ...

0693W00000NrxZcQAJ.jpg

Resolved! STM32 Bus Matrix behavior and arbitration mechanism

Hi,I'm trying to learn DMA in depth, but I'm confused at some points. It's about Bus Matrix and Arbitration mechanism. In STM32F446RE, there are 2 DMA controller and each one has 1 peripheral bus and 1 memory bus. Question is not about memory bus of ...

0693W00000NrmDBQAZ.jpg
MSara.2 by Associate
  • 4193 Views
  • 4 replies
  • 0 kudos