User Activity

Hello, if configure stm32g4 in up-down counting mode, does it support external events,such as external pin event or analog comparator events?for example ,rising edge of analog comparator event set TA1 output in up count directionand the same event re...
Does stm32g4 HRTIM support generate phase shift full bridge PWM with Peak current mode control, including peripherals HRTIM ,DAC,CMPx ?
Posted on April 04, 2018 at 06:45I tested K2 GTM tom0 channel based on studio version 5.7.2.for example ,tom0 ch0 output 20khz,50% ouput on io port selected in pin  -> it is OK,if I configure tom0_ch0,ch1,ch2,ch3 with same frequence and duty ,and ou...
Posted on March 20, 2018 at 06:46Does SPC5studio support print debug message on CONSOLE window by coding, not print message on serial port?
Kudos from