STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I am using NUCLEO-H723ZG and I am trying to use SPI the spi3 as SPI MASTER to the SPI SALVE device without success using DMA. I see the perfect data in the MISO line, But I unable to receive it into the "rx_buf", always "ZERO".

static void MX_SPI1_Init(void){ /* SPI3 parameter configuration*/ SpiHandle.Instance = SPI1; SpiHandle.Init.Mode = SPI_MODE_MASTER; SpiHandle.Init.Direction = SPI_DIRECTION_2LINES; SpiHandle.Init.DataSize = SPI_DATASIZE_8BIT; SpiHandle.Init.CLK...

0693W00000QKPAFQA5.jpg
ESega.1 by Associate II
  • 857 Views
  • 0 replies
  • 0 kudos

I'm getting sporadic I2C bus errors with no terminating ACK

I'm using STM32H743 I2C1 and FW as of december 2021.I'm testing in continous loop PMBus communication (straight I2C master interface).Appr. all 8h I'm getting a sporadic bus error.A good transaction looks like:this is a register read (addr-len=1) for...

0693W00000QKNvTQAX.png 0693W00000QKNwlQAH.png
BDimk.1 by Associate II
  • 2666 Views
  • 4 replies
  • 0 kudos

STM32H743 Config JTAG PB4 As Gpio Output?

hi when i use normal configuration for define this pin(PB4 in STM32H743) as GPIO output a problem occurs in the program.This pin is connected to the JTAG port and i use only SWD mode and pull up this pin by 10k to VCC.plz help me to config this pin a...

Natali by Associate III
  • 2201 Views
  • 5 replies
  • 0 kudos

STM32H750 flash access

Hi,I have two questions regarding STM32H750:1) I would like to pre-burn its internal flash with a simple code that enable XIP (execute in place) from external SPI flash and jump to some initial address on this external flash. Then I like to permanent...

EZido.1 by Associate
  • 920 Views
  • 0 replies
  • 0 kudos

Delay between UART TX frames at high speed

I am sending a fixed-sized buffer (512 byte) at 8 Mbits/s via UART out of an STM32F3, and I am experiencing what it seems to be a fixed delay (~ 2-3 bit periods) between consecutive frames. In the screenshot below, after sending the dummy value 01010...

LucaP by Associate III
  • 4292 Views
  • 4 replies
  • 0 kudos

What can cause an ADC calibration fails?

We are starting (difficultly due to the lack of devices) the pre-production of our system built around an STM32 H743VIT, and, on already two systems (out of about 50), we have failures initializing ADC 2. For the first one, replacing the MCU was succ...

JLojo by Senior
  • 7510 Views
  • 12 replies
  • 0 kudos

Driving TIM21 from 32KHz clock?

I've got a STM32L053 (on a Nucleo-Lo53R8). I'd like to drive TIM21 from the 32KHz clock, and gang it with TIM22 to form a 32 bit counter. But I'm confused on a few points.First question: how to drive TIM21 from 32KHz? The documents (RCC chapter, 7.2....

Resolved! HRTIM register update with Burst DMA doesn't work properly

The problem is as follows: When I am trying to update HRTIM master timer registers (MPER, MCMP1-4) on the STM32G474 via Burst DMA access, every data word I write into the BDMADR register gets written into two of the specified master timer registers. ...

DDPS.1 by Associate II
  • 2428 Views
  • 5 replies
  • 0 kudos