STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to connect STM32F407G-DISC1 by SWD to JTrace Pro / JLink

Hello,I have an STM32F407G-DISC1 evaluation board which I have been trying to connect to through SWD with a Segger JTrace Pro, but I haven't been able to connect to the board for some reason. I have been following a Segger provided document for the c...

DLlan.1 by Associate II
  • 3790 Views
  • 6 replies
  • 0 kudos

STLINK_V3 SET how to use for Custome board?

Hello, I am working on STM32H7 . I have custome board , I have to use the STLINK_V3 SET, which things that I need to consider for the programming through STLINK. How much vtg I have to set 3V/5V , In stm32Cube ide which setting I have to make. Can u ...

MDeva.1 by Associate II
  • 820 Views
  • 1 replies
  • 0 kudos

stm32f746 disco uImage port fail using TFTP

hi,i'm trying to port uclinux into the 746 disco board for studyhere is my settingsboard ip 192.168.5.100tftp server ip 192.168.5.120i've used window tftp toolbut, it was failed to port uImage into the board using TFTPi attached image that i 'm stuck...

Fish by Associate II
  • 942 Views
  • 0 replies
  • 0 kudos

Unstable BLE connection on STM32WB55 IC

This is my first attempt to ask a question here and my first time to use STM32WB55 platform, so I will try my best to put as many details as I can.I am using an STM32WB55 IC for a BLE project on a custom board. I installed the version v1.13.3 of stm3...

0693W00000QLz5hQAD.png 0693W00000QLz5mQAD.png

Resolved! STM32H7 Run* mode before configuring PWR_CR3

We are using the STM32H745 in one of our projects. We are using "LDO supply" mode (configuration 1 in Fig. 22 from RM0399 v3). Section 7.4 of RM0399 describes the power-up sequence, including a Run* mode where application code starts executing but ...