STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL_UART_RECEIVE_IT not working all the time in HAL

Hi,I'm using the UART functionality in NUCLEO-H745ZI-Q board. I want to transmit with UART polling and receive with interrupt. Every time I am able to transmit the characters on to the putty but sometimes receive interrupt is not working. I'm using H...

Mr. AK by Associate III
  • 2076 Views
  • 4 replies
  • 0 kudos

Timer external clock with interrupt

I have connected an external clock to TIM1 and I want to count the values ​​where the counter register is overflow with interrupt. My code is like this, but it doesn't work. TIM_ICInitStructure.TIM_Channel = TIM_Channel_2; TIM_ICInitStructure.TIM_ICP...

hdemi.1 by Associate III
  • 736 Views
  • 0 replies
  • 0 kudos

Resolved! The STM32 Selection Guide 2021 Shows that STM32F407VET6 contains 512K flash, but actually the flash could be wroten from address 0x0800 0000 to the 0x080F FFFF, So what's the problem?!

The STM32 Selection Guide 2021 Shows that STM32F407VET6 contains 512K flash, but actually the flash could be wroten from address 0x0800 0000 to the 0x080F FFFF, So what's the problem?! 

Resolved! Will software of STM32F407ZET6 work in STM32F407ZGT6?

Dear Community,I would like to request manufacturing additional board for a project but currently PCB assembling partner doesn't have STM32F407ZET6 in stock but it has STM32F407ZGT6.Basically, these two MCUs have the same capabilities except ZGT6 has...

VaZso by Associate III
  • 2749 Views
  • 3 replies
  • 0 kudos

I want to generate ONE PULSE TRIGGER by comparing the encoder counts input from 2MHz to 4MHz and setting the delay time and duty.

hello.​I want to generate ONE PULSE TRIGGER by comparing the encoder counts input from 2MHz to 4MHz and setting the delay time and duty.​Currently on TIM6void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim) is used and trigger is generated usi...

rm.1 by Associate II
  • 1932 Views
  • 4 replies
  • 0 kudos

STM32L011K4T - MCU ADC Temperature

Posted on February 06, 2018 at 01:23 Hi, I would like someone to confirm that the temperature I am getting is somewhat in the ballpark to be expected. If it isn't, could someone check my values that I am using from the datasheet? I am curre...

0690X00000609cnQAA.png
Nolan L by Associate III
  • 3705 Views
  • 4 replies
  • 0 kudos

STM32H7 Unique 96-bit serial number is really Unique ??

We are looking for Unique identification number per STM32, in the process we came to know about unique 96-bit serial number. is it really Unique ?? how it Guarantees, that no duplicate exist ??Can you please help on this clarification ??INFO

0693W00000UFS83QAH.png
SPati.7 by Associate III
  • 2412 Views
  • 4 replies
  • 0 kudos