STM32L5 FDCAN Message RAM access failure
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-04-19 5:01 AM
Hello,
I've been using the STM32L5 FDCAN HAL Driver but I have some problems with it.
When i try sending some CAN 2.0 frames to the STM32, an isr is called and the error Message RAM access failure is raised.
Sometimes, the ACK is sent but the interrupt is not even called.
if( HAL_FDCAN_ActivateNotification( &hfdcan1 , FDCAN_IT_LIST_RX_FIFO0 | FDCAN_IT_GROUP_RX_FIFO0 , (uint32_t) NULL ) != HAL_OK ){
monitor_errorHandler( MONITOR_CRITICAL_FAULT( 16 ) , 1 );
}
if( HAL_FDCAN_ActivateNotification( &hfdcan1 , FDCAN_IT_GROUP_RX_FIFO1 , (uint32_t) NULL ) != HAL_OK ){
monitor_errorHandler( MONITOR_CRITICAL_FAULT( 16 ) , 20 );
}
if( HAL_FDCAN_ActivateNotification( &hfdcan1 , FDCAN_IT_GROUP_TX_FIFO_ERROR | FDCAN_IT_GROUP_MISC | FDCAN_IT_GROUP_BIT_LINE_ERROR | FDCAN_IT_GROUP_PROTOCOL_ERROR , (uint32_t) NULL ) != HAL_OK ){
monitor_errorHandler( MONITOR_CRITICAL_FAULT( 16 ) , 2 );
}
if( HAL_FDCAN_ActivateNotification( &hfdcan1 , FDCAN_IT_TX_COMPLETE , FDCAN_TX_BUFFER0|FDCAN_TX_BUFFER1|FDCAN_TX_BUFFER2 ) != HAL_OK ){
monitor_errorHandler( MONITOR_CRITICAL_FAULT( 16 ) , 3 );
}
/*
* Gestion Erreur CAN
*/
if( HAL_FDCAN_ActivateNotification( &hfdcan1 , FDCAN_IT_LIST_TX_FIFO_ERROR , (uint32_t) NULL ) != HAL_OK ){
monitor_errorHandler( MONITOR_CRITICAL_FAULT( 16 ) , 4 );
}
if( HAL_FDCAN_ActivateNotification( &hfdcan1 , FDCAN_IT_LIST_MISC , (uint32_t) NULL ) != HAL_OK ){
monitor_errorHandler( MONITOR_CRITICAL_FAULT( 16 ) , 5 );
}
if( HAL_FDCAN_ActivateNotification( &hfdcan1 , FDCAN_IT_LIST_BIT_LINE_ERROR | FDCAN_IT_GROUP_BIT_LINE_ERROR ,(uint32_t) NULL ) != HAL_OK ){
monitor_errorHandler( MONITOR_CRITICAL_FAULT( 16 ) , 6 );
}
if( HAL_FDCAN_ConfigGlobalFilter(&hfdcan1, FDCAN_REJECT, FDCAN_REJECT, FDCAN_REJECT_REMOTE, FDCAN_REJECT_REMOTE) != HAL_OK ){
monitor_errorHandler( MONITOR_CRITICAL_FAULT( 16 ) , 7 );
}
Labels:
- Labels:
-
FDCAN
-
RAM
-
STM32L5 Series
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-04-19 6:21 AM
As for the initialisation code, the FDCAN1's clock is 110 MHz :
hfdcan1.Instance = FDCAN1;
hfdcan1.Init.ClockDivider = FDCAN_CLOCK_DIV1;
hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;
hfdcan1.Init.AutoRetransmission = ENABLE;
hfdcan1.Init.TransmitPause = DISABLE;
hfdcan1.Init.ProtocolException = ENABLE;
hfdcan1.Init.NominalPrescaler = 2;
hfdcan1.Init.NominalSyncJumpWidth = 8;
hfdcan1.Init.NominalTimeSeg1 = 40;
hfdcan1.Init.NominalTimeSeg2 = 14;
hfdcan1.Init.DataPrescaler = 5;
hfdcan1.Init.DataSyncJumpWidth = 6;
hfdcan1.Init.DataTimeSeg1 = 16;
hfdcan1.Init.DataTimeSeg2 = 6;
hfdcan1.Init.StdFiltersNbr = 28;
hfdcan1.Init.ExtFiltersNbr = 0;
hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK)
{
Error_Handler();
}