STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-NUCLEO-IDB05A2 not working, stuck on SPI_Reset on STM32F746ZG

Hi all, hope all is well. I've been trying to learn the STM32 by creating a project for myself, and I am stuck on the bluetooth portion of things. I have watched videos, read documentation, etc, and I just don't know where I'm going wrong. I've been ...

TC2 by Associate II
  • 3850 Views
  • 6 replies
  • 0 kudos

spi5 will not do less then 8 multiplier.

I set up my spi5 as follows hspi5.Init.Mode = SPI_MODE_MASTER; hspi5.Init.Direction = SPI_DIRECTION_2LINES; hspi5.Init.DataSize = SPI_DATASIZE_8BIT; hspi5.Init.CLKPolarity = SPI_POLARITY_LOW; hspi5.Init.CLKPhase = SPI_PHASE_2EDGE; hspi5.Ini...

ulao by Associate III
  • 1805 Views
  • 9 replies
  • 0 kudos

I am using STM32L443 processor. When the processor is locked, I reset the processor with NRST with external wdg. The processor is not reset although WDG is working properly.

I checked WDG. The system is working properly. If there is no reset, it resets when I disable the WDG signal. In case of deadlock, I pull to GND myself, but it still does not reset. The only solution is to cut off all energy.

OŞeno.1 by Associate II
  • 2407 Views
  • 5 replies
  • 0 kudos

When I program my device in debugging via JTAG/SWD with instances of low-power STOP mode within the code and disconnect Debugger, device never goes to sleep and get Ghost wake-up INTs. However, if I power cycle not pin reset device, every thing works.

Is there registers set by JTAG/SWD preventing sleep after programming.I also experience the same behavior after programming and reset within the STM32 ST-LINK Utility and not only within the IDE

UAnya.1 by Associate II
  • 2807 Views
  • 5 replies
  • 0 kudos

stm32g474 interrupt problem

Hi allI have a problem with interrupts on my STM32G474VEH6 based board. Timer 6 generates an interrupt every 1ms. Program crash at HAL_TIM_Base_Start_IT(&htim6);But after resetting the power of the board, the software starts working correctly.The sam...

RHert.1 by Associate II
  • 2881 Views
  • 5 replies
  • 0 kudos

Resolved! What is the letters -RBT6 -means in STM32G070RBT6 ?

Hey, I am working on STM32G070 development board.i downloaded from the orcad resources the scheme for the processor.however i can see it has additional letters and digits on the headercan someone explain me what are the meaninig of them?

0693W00000WLPKGQA5.png
YShko.1 by Associate II
  • 1554 Views
  • 2 replies
  • 0 kudos