User Activity

I saw multiple resources on different conversions between chips, such as AN5094 (between F3 and G4), but I can't find anything for G4 to F7.Is there a step by step process to follow that has a program do most of the work, something similar to MCSDK, ...
Opening the example ACIM-STM32G431 .ioc file in a text editor (notepad) shows hundreds of hidden options:I am trying to imitate it through CubeMX, but the parameter settings are not listed under MotorControl. I have matched all the other parameters. ...
After getting the example ACIM program running (Nucleo-G431RB and STEVAL-IHM023V3), I want to customize beyond those two boards. To do this, I believe I need to generate (or hand-make) a .ioc file.Trying to generate a file through MC WorkBench just ...
Unfortunately, I cannot get MCSDK to generate the Middleware with the Induction option, as it either does not appear (v. 6.0.0) or it fails to generate pwm_curr_fdbk.c properly (v. 5.Y.4). The other two algorithms generate fine and can run my setups....
What is the difference between modes Enabled, Six-Step, and Induction in STM32CubeMX?Documentation is lacking
Kudos from