STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7 CPU runs too slowly occasionally

test code as below:#include <rtthread.h> #include <rthw.h>   #define CPU_USAGE_CALC_TICK 100 #define CPU_USAGE_LOOP 100   static rt_uint8_t cpu_usage_major = 0, cpu_usage_minor= 0; static rt_uint32_t total_count = 0; static rt_uint32_t _c...

0693W00000Y9b8LQAR.png 0693W00000Y9b9TQAR.png
zhuij.1 by Associate II
  • 2545 Views
  • 4 replies
  • 0 kudos

Possible DMA reading problem from ADCx_CDR

Dear All,I am trying to develop a code for STM32H742VGT revision V. ADC1 and ADC2 work in regular simultaneous mode and they are set to convert 6 channels. All the settings are exactly same to have same sampling and conversion time. Of course, ADC1 a...

0693W00000Y9gWIQAZ.png
TA1 by Senior
  • 1332 Views
  • 0 replies
  • 0 kudos

Resolved! SPI interface issues on STM32U575VGT

I´m using the SPI1 via the alternative pins PB3-PB5 and I'm experiencing various issues. I have previously used the STM32F722 with somehow same CubeIDE setup and code and that works perfectly.I have made a simple test application that only sends one ...

MJens.2 by Associate II
  • 3283 Views
  • 5 replies
  • 0 kudos

STMod+ on H757I-EVAL Board

Hey Folks.So, I have the H757I-Eval Board that I got as a gift, and given that I'd like to try some stuff and even follow some tutorials, I miss the exposition of the PINs. Reading TN1238 which talks about a fan-out expansion board, it says "The prin...

0693W00000Y9g1jQAB.jpg
nnoK by Associate
  • 1165 Views
  • 1 replies
  • 0 kudos

DMA SPI transfer recovery time

I am making this call:  if(HAL_SPI_Receive_DMA(&hspi3, &aRecvBuffer[0],3)!= HAL_OK)inside an external GPIO interrupt handler that gets called every 20 us. It is used to read data from an external ADC. I noticed that this dma transfer works well only ...

fma23 by Associate II
  • 1516 Views
  • 2 replies
  • 0 kudos

Resolved! STM32U585 OSPI hard fault on memory-mapped write

I'm trying to follow the OSPI_NOR_MemoryMapped STM32CubeIDE example, but for a different device (W25Q128FV). Write Enable, Read Status, and Erase Sector commands behave as expected, as well as memory-mapped reads. This has been confirmed by monitorin...

BHamm by Associate II
  • 5983 Views
  • 9 replies
  • 0 kudos

copy float's binary content into uint32_t

Hello,I am trying to copy the content of a float variable with memcpy into uint32_t variable. unfortunately the binary content changes after copying. it should be 0xfff00000, like in the float variable. Does anyone know why this happens and how can I...

NTaha.1 by Associate II
  • 4278 Views
  • 4 replies
  • 0 kudos