User Activity

When enabled Data cache for example in main:/* Enable D-Cache---------------------------------------------------------*/ SCB_EnableDCache();I think I am supposed to uncomment L63 in sd_diskio.c to activate Cache maintenance:/* USER CODE BEGIN enabl...
I am working on a custom board equipped with an STM32H753 and a SD-Card connected via SDMMC 4bit wide Bus. FreeRTOS is used. HAL is generated using CubeMX and the package "STM32Cube FW_H7 V1.9.1".CubeMX generates the file sd_diskio.c and in it (line ...
For a STM32L433CB I generated the Custom HID code using CubeMX version 6.2.1 and the Cube FW_L4 V1.17.0The CUSTOM_HID_FS_BINTERVAL   is set to 5ms and I placed a Custom HID Descriptor. Also I adjusted USBD_CUSTOMHID_OUTREPORT_BUF_SIZE and USBD_CUSTOM...
Kudos from
Kudos given to