STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

charger detect problem

Hello,I’m using STM32L412RB.I'm trying to differentiate between the types of chargersWhen the charger is connected, reboot occurs, and I run HAL_PCDEx_ActivateBCD()/HAL_PCDEx_BCD_VBUSDetect() in MX_USB_DEVICE_Init().After that, in case of abnormalit...

MKim.12 by Associate II
  • 1293 Views
  • 0 replies
  • 1 kudos

Firmware Protection (F1 Series)

Hello dear! I'm developing a new product. I would like use the STM32 F1 series, but I was surprised with this: https://blog.zapb.de/stm32f1-exceptional-failure/The F1 Series don't have RDP Level 2 protection, in this case, what's the most security wa...

STM32U5 ADC specifications?

I am planning to use ADC with 16 bits achieved using oversampling in STM32U5.But on Datasheet there is no data wrt to ADC oversampling.Can somebody help me with data regarding ENOB, EL,ED when ADC is oversampled. Datasheet : DS13737Datasheet - STM32U...

Shru2 by Associate II
  • 1449 Views
  • 1 replies
  • 1 kudos

Resolved! EXTI interruption flags

Hi.I am having some issues trying to use the EXTI module, to implement interruption routines associated to ports.The problem is related to the behavior of STM32 microcontrollers with ports interruptions. In most microcontrollers (i.e. Texas Instrumen...

JNava.1 by Associate II
  • 9903 Views
  • 13 replies
  • 0 kudos

Resolved! If I want to control a relay via the TX of a UART do I just connect the appropriate STM32 pin to the relay? Or is there anything else I need to do (besides programming)?

I'm looking to use a ITS4200S-ME-P relay to switch a high voltage signal and would like to control that via a UART. Per the datasheet this relay, "can be switched on and off with standard logic ground related logic signal at pin IN."

DMill.16 by Associate II
  • 4035 Views
  • 5 replies
  • 0 kudos

Resolved! STM32G4: ADC sampling and hold capacitor value

SetupSTM32G491KEADC1 Input Channel 3 using Pin PA2Vdd = 3VRC-Filter at the ADC input with R = 33 Ohm, C = 330 pFObservationWhen measuring the voltage at the ADC input with an oscilloscope, we see the voltage drop caused by switching the input signal ...

tssh by Associate
  • 7697 Views
  • 4 replies
  • 3 kudos

Resolved! Executing main() by XIP with W25Q32 QSPI Flash

HiI'm using STM32H750VBT6 with W25Q32 QSPI external flash memory from Winbond and I'm using Keil Microvision IDE with ARM_CC Compiler.I'm trying to execute my whole project from the QSPI flash directly (which is called XIP). I know that I have to con...

Farbod by Associate
  • 2796 Views
  • 2 replies
  • 0 kudos