STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to write doublewords to flash on an STM32F411RE

I could get HAL_FLASH_Program to write WORDS, as soon as I moved to FLASH_TYPEPROGRAM_DOUBLEWORD the last error returned is alwasy PGA | PGS flags in the SR. PGA = alignment, PGS = sequence. I referred to every internet article I could to figure out ...

ELeyl.1 by Associate II
  • 2501 Views
  • 1 replies
  • 0 kudos

Resolved! UART DMA Transmitter and receiver issue

i'm using STM32F730 as uart receiver and STM32f0 as uart transmitter baud rate 9600, 8 bit data representation. i'm using DMA with interrupt for the communication. i'm using HAL for programming on IAR workbench. The transmitter is continuously transm...

NSing.5 by Senior
  • 1717 Views
  • 2 replies
  • 1 kudos

Hard fault invalid state

I'm trying to inject a simple wrapper around my timer interrput handler written in C - primarily for debug purposes to simplify debugging the state of registers and stack before the C code gets in and messes up the stack and state pushing all the jun...

ShawnP by Associate III
  • 4718 Views
  • 8 replies
  • 0 kudos

Resolved! Looking for solution to hard fault when using UART to transmit. Particularly, when it calls HAL_GetTick() in Uart function

Hi all,I am using Nucleo-L552 Evaluation board running , CMSIS_RTOSV2 (FreeRTOS), firmware STM32Cube FW_L5 V1.3.0. Debugging via built-in ST-Link. I have a Hard fault on HAL_GetTick() when running UART transmit on one of the threads. It debugs fine w...

TDinh.1 by Associate II
  • 7112 Views
  • 7 replies
  • 0 kudos

Resolved! How to get the PVD state on the STM32L4xx ?

Sir,I am using the STM32L432 for my project.How to get the PVD state ?I want to know the power voltage that is above the level or under the level.Thanks.void HAL_PWR_PVDCallback(void) { if ( __HAL_PWR_PVD_EXTI_GET_FLAG() ) { // TODO: get ...

JLiao by Associate II
  • 2014 Views
  • 2 replies
  • 0 kudos

How to make ınput capture with STM32g030f6t6?

Hi everyone, I'm trying to use Input Capture with 1 Timer by using both edges option as external. I'm new at this microcontroller and I could not understand how to make it correctly with HAL library. Can anyone help me how to do?

MÇETİ.1 by Associate III
  • 2762 Views
  • 7 replies
  • 1 kudos