STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

H757 code to reboot both cores

I am using a H757 processor and i would like to reboot both cores (M4 & M7) from the M7 running code.Would anyone be able to help ? As i can’t find a definitive answer about how to do it.thanks

UART Data Getting DMA'd In Wrong Order After First Packet

I have a device that receives six bytes via the UART. There is a known SOF and EOF byte. The first time I get the data, all is well. But subsequent receptions are "corrupted": either the EOF byte is first, or sometimes I get two SOF bytes in a row (a...

nobbyv77 by Associate II
  • 2205 Views
  • 2 replies
  • 0 kudos

SPI example on Nucleo-g474

I'm using a Nucleo-g474REI want to use a timer / DMA to trigger a SPI Rx only transfer to memory.I need to transfer two 9 bit words every trigger, 1 uSecs, and 4096 two word transfersCan anyone point me to an MX cube example?

LHarm.1 by Associate III
  • 2505 Views
  • 3 replies
  • 0 kudos

HAL _QSPI_ERROR_TIMEOUT in NOR flash memory

Hello,currently i am working on stm32f4113 and nor flash(w25q128) using QuadSPI 1st time i erase the 1st block i get no error but 2nd time i erase any block i get  HAL_QSPI_ERROR_TIMEOUT.i get error in this function QSPI_WaitFlagStateUntilTimeout(hq...

AA.27 by Associate II
  • 2202 Views
  • 1 replies
  • 0 kudos