STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SMPS on STM32N657

Hello,Regarding the STM32N657, I'm not using the internal SMPS.  My question is:  Do we need to put capacitors on the 6 VDDSMPS pins or can they be left as no connect?   Same question on the VLXSMPS pins... do we need the capacitors on these pins, or...

mattcrc_0-1761592495500.png
matt-crc by Senior III
  • 941 Views
  • 8 replies
  • 1 kudos

Resolved! STM32U031 freezing IWDG counter in STOP 0 mode.

Hello Everyone,I am facing an issue with my MCU entering low-power mode.My idea is to freeze the Independent Watchdog (IWDG) counter in STOP mode so that the MCU will not reset due to the IWDG counter elapsing.From my understanding, this can be achie...

sureshkumar1_0-1761636863691.png

Resolved! STM32N657 IO 3.3V tolerant?

Hello,I'm using the STM32N657 processor and have the HEXASPI device running at 1.8V.  VDDIO2 is connected to 1V8 supply (which affects: PO[5..0] and PP[15..0]The FMC is placing the A23 line on pin PO1 (this is the only option for the FMC-A23) and the...

mattcrc_0-1761602911315.png
matt-crc by Senior III
  • 646 Views
  • 5 replies
  • 1 kudos

Resolved! L073: ADC & DMA, strange buffer "shift" in CIRCULAR mode

Heyho,strange things happening that I'd like to understand for a STM32L073 (Nucleo for now).Setup on a L073 @ 32MHz:- ADC is clocked by PCLK/4- ADC prescaler = 2 -> divide by 4 -> 2 MHz- 12 bit right aligned- ref V = VDDA = 3.3V- hardware oversamplin...

LCE by Principal II
  • 1346 Views
  • 15 replies
  • 2 kudos

Resolved! STM32H750 XiP Clock change

Hey together, I have a question regarding changing the clock while running in XiP mode. Upfront everything works so far very well. On our STM32H750 we have a very simple bootloader. This bootloader configures the QSPI and the STM32H7 to run the appli...

ESawa1_0-1761134946554.png
ESawa.1 by Senior
  • 1130 Views
  • 6 replies
  • 0 kudos