STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F410 PLL Jitter on PWM

Hello,i want to use a really precise PWM signal but i get a lot of Jitter on it.I am using the F410 with a 16Mhz crystal. The PLL produces from there a Frequency of 100Mhz (I need this high frequency for my other tasks).The rest of my hardware needs ...

PDieh.1 by Associate III
  • 13489 Views
  • 26 replies
  • 1 kudos

LSM6DSO

I want to read Temperature data in register [20h,21h] , but the data I read are 0x00 , should I setting which register ?  

KevinHSU by Associate
  • 2116 Views
  • 3 replies
  • 1 kudos

Resolved! Issue with STM32F107VCT6 Data Corruption when Resetting nRESET

Hello,I am using the STM32F107VCT6 microcontroller and, under normal circumstances, it works flawlessly. However, I have been encountering an issue where data in a specific memory area becomes corrupted when I toggle the nRESET pin at 2-3 second inte...

NS by Associate II
  • 2016 Views
  • 5 replies
  • 0 kudos

Resolved! Some I3C Speed Rates are not available?

Hi,I am working with  STM32H5RBT6U:How do I calculate the frequency of the I3C Controller? Is there documentation to cover the content?I tried using CubeMX to set the frequency, but strangely, all the frequencies work fine except 3~5MHz. The exceptio...

taylor_quan_1-1697423865215.png taylor_quan_0-1697423823825.png taylor_quan_3-1697424211112.jpeg

Resolved! RTC Alarm EventCallback called only 1 time

Working with the RTC I'm having some issue with the callback only being called a single time. void HAL_RTC_AlarmAEventCallback(RTC_HandleTypeDef *hrtc) { RTC_AlarmTypeDef sAlarm; uint32_t hobb_time; __HAL_RTC_ALARM_CLEAR_FLAG(hrtc, RTC_FLAG_AL...

Resolved! Has there been any changes to TIMx_SMCR in STM32F407 series MCUs?

This might be a really stupid question but I recently downloaded RM0090 revision.19 for reference in use of timers in STM32F407IGT6.But I have noticed some diffrences from old reference manual & I can't find revision history for that. Old revision of...

SMCR_OLD.png SMCR_NEW.png
jhson by Associate
  • 3832 Views
  • 5 replies
  • 10 kudos

Square wave of 2, 4, 8 Mhz generation.

Posted on January 09, 2015 at 16:49Hi I'm a newbie to stm32 , I have a STM32F4 Discovery board with me. So what I want to do is to generate 2Mhz,4Mhz,8Mhz square wave  on any of the Pins on the Header. Can you please provide some sample code for th...

STM32H7 - Unable to use PA15 as GPIO output pin

I'm using an STM32H725ZE chip. I know that PA15 defaults to JTAG pin JTDI, but the datasheet for the part specifically says this:In SW-DP mode, the unused JTAG lines JTDI, JTDO and nJTRST can be used for otherfunctions.I'm in SWD mode because it's a ...

FredB by Associate II
  • 3603 Views
  • 5 replies
  • 0 kudos

Cant access RTC coming out of standby mode

Hi  I am programming a STM32L433 and have the processor wakeup from Standby mode. The first thing it does after wakeup is check the cause of the wakeup, and if RTC increase the time, do a few readings and go back into Standby mode. When I am running ...