Question
PC13/PC14/PC15 pins on the STM32F103CBT6 usage
Hello,
I have a question related to the GPIOs PC13/PC14/PC15. Due to the fact that in my project I am running out of the other GPIO pins I have a question related to those pins above. I know that those pins have limitation to max 3mA sink current so do you see a problem to use them to drive LED ( I need to create a heart bit for the MCU ) where I will use LED and limit the forward current to 2-2.5mA ?
Thank you in advance
Jacek