STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Read data from PC to STM32 via USB CDC

Posted on February 24, 2016 at 06:02 I am working on a project. One of the part is exchanging data between PC and MCU(STM32F4) via the USB CDC. Sending data from STM32 to PC is very easy, but there is difficulty receiving data from PC. ...

rwmao by Senior
  • 25380 Views
  • 18 replies
  • 2 kudos

Resolved! CRC_POLYLENGTH_16B undeclared in STM32F030CCTx

In `STM32F030CCTx` I need to set the CRC in 16-bit length by calling HAL_CRCEx_Polynomial_Set(MATRIX_UART_settings->crc, CRC_POLY, CRC_POLYLENGTH_16B); but the compiler shows the error : 'CRC_POLYLENGTH_16B' undeclared (first use in this function) in...

Soad by Associate II
  • 2392 Views
  • 3 replies
  • 2 kudos

Resolved! STM32L4 - internal routing of opamp output to ADC

I'm trying to use the internal op-amps of an STM32L471 to amplify a small current-sense voltage before measuring it via ADC. This figure from the relevant product training resource shows an internal arrow labelled "ADC," coming from the op-amp output...

oscarw_0-1697771613803.png
oscarw by Associate II
  • 5042 Views
  • 3 replies
  • 2 kudos

Unable to program STM32F103 through UART

I created a custom board with the STM32 (F103C8T6), and I am trying to program it using a FTDI USB to Serial module. However, nothing is happening, it doesn't seem to be sending anything and when I try using STM32CubeProgrammer it says:Timeout error ...

Nv7_2-1694149065260.png Nv7_4-1694149113730.png
Nv7 by Associate III
  • 11308 Views
  • 13 replies
  • 1 kudos

CODEC with STM32

Hello, I would like to know how to retrieve the acquisition values ​​: INPUT -> ADC -> SAI -> µP like the diagram below : I have a program that works for this : DMA -> SAI -> DAC But this is not the way I would have wanted to make my CODEC work. Do ...

DYann1_0-1692602441481.png
DYann.1 by Senior II
  • 14153 Views
  • 30 replies
  • 0 kudos

Migrating from Nucleo-144 board to real IC

HI i m currently working on a H723 nucleo144 EVK, and have completed the coding and is contemplating to flash the code onto STM32H750IBK6. Question is whats the best way to port over the code (with .ioc) without recreate a new project,  new IC select...

Resolved! Blocking vs non-blocking UART using an RTOS

Hello there!I've been setting up the UART peripheral on my STM32H5 and everything works great! However, there is one thing I can't completely understand:Using an RTOS to call HAL_UART_Transmit or HAL_UART_Transmit_IT, what's the advantage of one over...

nunokisi by Associate II
  • 7742 Views
  • 4 replies
  • 1 kudos

Didn't get the same binaries with the same compiler

Hi everyone,I'm currently trying to build my project on two differents computers. My computers have not the same STM32CubeIDE: 1.13.1 and 1.11.2. Compilers are the same, I ckecked it with version 10.3-2021-10. Flags and options of compilation are the...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.