STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32N6 - Unable to reset using NRST pin

Hi,I am working with a custom board using an STM32N657X0H3Q and cannot for the life of me bring about a reset via the NRST pin.I have tried applying the workarounds from errata sheet ES0620 - Rev 3, sections 2.2.19 and 2.2.23, but my device still jus...

silvia_b by Associate II
  • 315 Views
  • 6 replies
  • 1 kudos

Resolved! STM32C011J4M - issue with pin overlapp

Hello to whom this might concern,I was recently experimenting with STM32C011J4M for a small hobby project (I am trying to fit into a about coin size) and want to comunnicate with other chip over I2C. Due the size of the package I cannot use debugging...

PWM input output drift

Hello everyone,I have an NUCLEO-H755I-Q with the following setup;i) A 50Hz PWM input pulse goes to HTIM1 in PWM input mode with DMA enabled in channel 2 so the moment CCR2 has captured some data they can be transferred,ii) HRTIMCHA2 with CMP1 enabled...

chrkaras by Associate III
  • 117 Views
  • 0 replies
  • 0 kudos

Resolved! STM32H753XIH6: VCAP internal connections

Hi I am trying to figure out these VCAP conections.From the datasheet I could look like they are internally connected together, for this reason could avoid routing these three pads together on my board.Can anybody confirm that is the case?Thank you.

tyassin_0-1778059248074.png
tyassin by Associate III
  • 153 Views
  • 3 replies
  • 5 kudos

Resolved! STM32F303RE and X-NUCLEO-IHM07M1 for FOC

Hello everyone,I am working on my bachelor thesis about sensorless Field-Oriented Control (FOC) for a three-phase BLDC motor.At the moment, I have a NUCLEO-F303RE board, a small BLDC motor, an ESC, and a power supply. I have already generated and mea...

erayGz by Associate
  • 151 Views
  • 1 replies
  • 1 kudos