cancel
Showing results for 
Search instead for 
Did you mean: 

Can I-CUBE-LRWAN be ported for other MCUs like F-series or G-series?

sheikhasif
Associate

I am curently using I-CUBE-LRWAN v2.1.0 package in STM32L476-Nucleo with HPD13A-Sx1276 Transreceiver to communicate with TTN network server & its working properly as it should be.

IMG_20230621_122002.jpgSTM32L476-NucleoSTM32L476-Nucleo

The point is I have STM32G431 & STM32F407, in which i want to port I-CUBE-LRWAN stack.

Is it possible to do so?

If Yes, How? (teach me like a noobie)

If No, Why?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

With the earlier LRWAN implementations it was possible. Certainly for the F4

The porting was as I recall somewhat involved. Clone the STM32 family specific files into ones for the target platform, bring in the HAL files for that platform. Adapt the pins and HAL calls to suit the board.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Can u please get me clear in this?

Is the dependency is LowPower only on L0, L1 & L4 boards or is there more to that. Why not other Low Powered boards like L5, U5 or any other boards by ST.