STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F407 RTC

I use the RTC of STM32F407 with LSE (32.768 kHz).A battery is connected to VBAT for backup.In the reference manual, the Backup operating voltage is at least 1.65V, but the RTC is actually backed up to about 0.3V.I do not know the reason. Could you te...

tyama.19 by Associate
  • 421 Views
  • 0 replies
  • 0 kudos

Multi slave SPI for STM32F427ZIT6

Hi,I am using STM32F427ZIT6 for one of the design. I am new to designing. I am connecting 8 ADC's to this device using SPI. I am using SPI4 (Pin 1,4,5). I want to know whether chip select (8 nos) can connect to any IO's?? Because NSS (slave select) i...

DKS by Associate II
  • 765 Views
  • 3 replies
  • 0 kudos

RTC periodic wake up interrupt fires only once

Posted on January 26, 2018 at 21:05 Hi, I'm writing an application with a STM32L051 (32 pin, 64kB ROM). This application uses the RTC and I wanted to use the RTC periodic auto wake-up feature to update the time display every 60 seconds. THE...

Fixed version of Cortex in STM32H7 ?

Hello,I've heard that some bugs have been found on Cortex M7 related to cache management, and that the STM32H7 will embed the fixed version of Cortex design. But I can't find when this updated version of STM32H7 will be available. Also, where (in wha...

Gpeti by Senior II
  • 1708 Views
  • 11 replies
  • 0 kudos

About FMC-SRAM transmission

hi ,I have some problms about FMC-SRAM with own r&d board based on stm32h750,hope someone give me some hlps�? Now we have a strange problem that we operate on an external 16-bit bus. If we just write a word (16-bit) that is 2 bytes, the actual bus op...

HLeaf by Associate
  • 827 Views
  • 3 replies
  • 0 kudos