STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1568 Views
  • 0 replies
  • 2 kudos

[STM32U575ZI-Q] Not able to set the USB OTG FS. The option(USBX) is disabled in the middleware section of CubeMx for USB OTG FS.

I am trying to set up USB OTG FS as CDC(virtual com port). For the other Nucleo board (Nucleo F746ZG) I was able to set it up in middleware section of CubeMx GUI. With the STM32U575ZI-Q board, the option(USBX) is disabled. Also, in the device manager...

pkulk.1 by Associate II
  • 5640 Views
  • 7 replies
  • 0 kudos

stm32cubemx failed to open ACCESS TO MCU SELECTOR

When I click ACCESS TO MCU SELECTOR, the console prints : 2023-01-18 14:35:27,011 [INFO] MultiScanPanel:196 - Auto-refresh data requested => check proxy status ongoing 2023-01-18 14:35:27,014 [INFO] FinderPluginLoader:92 - Searching for filters in in...

0693W00000Y8V7jQAF.png
yl.1 by Associate
  • 2627 Views
  • 2 replies
  • 0 kudos

Resolved! SD Card option not present for SDMMC2

I have followed this tutorial and gotten FATFS working perfectly on the Nucleo-L4R5ZI-P however I am trying to transfer my code to the STM32L4Q5CGU6 and the option under;middleware -> FATFS -> FATFS Mode and Configuration -> there is no option for SD...

_legacyfs_online_stmicro_images_0693W00000bkx6mQAA.png
HBegn.1 by Associate
  • 3326 Views
  • 4 replies
  • 0 kudos

Resolved! Cannot enable SPI1 on F427

Hi,I cannot enable SPI1 interface in CubeMX with STM32F427.I only see the message "I2S1" must be disabled":But I2S is not used in my project.In Pinout view it is possible to select Pins PA4 to PA5 and PB5 for SPI1-sugnals without error messages.Whats...

ReinhardD_0-1697102015927.png

Resolved! STM32U575

Hello. I have been dealing with USBx host HID application for a while trying to find a soluction to my problem but despite that I dont know what else to look for to make it work. I'm working with Cube 6.9.2 and with its lastest library STM32Cube_FW_U...