cancel
Showing results for 
Search instead for 
Did you mean: 

I am currently working on OTG mode in USB Communication. In that the USB_FS_IRQHandler function is not invoked correctly, Is this because of functions inside the IRQ handler are not properly defined or some functions are missing?

pvall.1
Associate II
This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8
waclawek.jan
Super User

Which STM32?

What do you mean by "not invoked correctly"?

JW

STM32 NUCLEO-L4P5ZG.

"Not invoked correctly" means debugging control line entering into Infinite loop.

waclawek.jan
Super User

What is "debugging control line" and where is that infinite loop?

JW​

Debugging control line is the one which is used in STM Cube IDE for debugging.

Infinite loop is While(1)

Wijeden RHIMI
ST Employee

Hello @pvall.1,

Could you please inform us which Cube IDE version and MX ? and have a look at the map file in the project and search for USB_FS_IRQHandler 

  • Where is this object sourced from?

 Wijeden,

Cube IDE version is 1.11.0

In the map file it is mentioned like this

.text.OTG_FS_IRQHandler

        0x000000000801faf4   0x15c ./src/USB.o

        0x000000000801faf4        OTG_FS_IRQHandler

Wijeden RHIMI
ST Employee

Hello@pvall.1 ,

Could you please provide a screenshot of the debug session where the infinite loop?

Wijeden,

Hi ,

It's working now I sorted out the issue.