STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1588 Views
  • 0 replies
  • 2 kudos

I2C - generated CubeMX

Posted on March 28, 2017 at 22:56Hello, I still tried with I2C on nucleo F401RE. I am use STM32CubeMx for generate files, but my program is not working. I  want send three bytes on I2C in blovking mode. This is my code: I2C not working, still is log...

Sigh - another CubeMX bug...

Posted on February 27, 2018 at 01:04Version 4.24.0 STM32CubeMX - STM32F303RCTx has pin 18 as PF4 instead VSS - thought I had an extra signal!!#cubemx-v4.24

Bug reporting: USB CDC: Using non-initialized dynamic memory

Posted on February 25, 2018 at 00:06DUT:Device: STM32F407VGTBoard: STM32F4-DISCOVERYPC part:OS: Windows 10Driver: USB Serial Device, Microsoft, 6/21/2006, v10.0.16299.15Initialization code is generated using the STM32CubeMX Version 4.24.0 with STM32...

zoromgerg by Associate II
  • 1746 Views
  • 3 replies
  • 0 kudos

Why is HAL documentation lacking?

Posted on February 02, 2017 at 11:40The ST HAL should make programming STM32 microcontrollers easier. After all, it is a 'Hardware Abstraction Layer'. It provides an interface to the user, so he doesn't need to manipulate the hardware registers dire...

[proposal] Public STM32CubeMX issue tracker

Posted on December 14, 2017 at 13:10There are lot of bugs in STM32CubeMX and its components. Having public issue tracker will simplify the situation with reporting all issues and tracking their status.Idally, having public source code of STM32CubeMX...