cancel
Showing results for 
Search instead for 
Did you mean: 

LL_USART_Init generated by CubeMX size reduction ?

WGend.15
Associate III

Hi everyone,

Like most of embedded work, our project aims to have the smallest size possible.

Looking at what I can optimize, I came across the LL_USART_Init function that is generated by CubeMx.

This function uses LL_USART-SetBaudRate which needs to use Division for unsigned long (_udivmoddi4). On a STM32F4 project, _udivmoddi4 takes 720 bytes of flash space!!

Does anyone have a simple trick to get around this apart from getting rid of CubeMX initialisation and never use LL_USART_SetBaudRate ?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
gbm
Principal

If the target baud rate is constant - just define the clock frequency as a constant (forget the variable) and use constant expression to initialize BRR:

#define USART_CLK 48000000u

#define BAUD_RATE 115200u

USART1->BRR = (USART_CLK + BAUD_RATE / 2) / BAUD_RATE;

USART1->CR1 = USART_CR1_TE | USART_CR1_RE | USART_CR1_UE;

These two lines are enough for simple UART init, so you may also forget any fancy HAL/LL UART_Init routines.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice