STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1535 Views
  • 0 replies
  • 2 kudos

Resolved! I cannot enable DCMIPP interface pins

Hi,I am implementing DCMIPP configuration in that I am enabling the CSI but when I trying to enable the pin I cannot enable the the camera pins those pins are showing red. And I am unable locate .ioc file  for DCMIPP interface is there any .ioc file ...

Resolved! Missing files in generated code for USB Audio

Question for STM.Could you please advise what to do to make the environment generate audio files?Could anyone of you show me how to generate these files?They are generated for all classes except audio.I guess there should be these too.Alternatively, ...

image.png
konsul41 by Associate II
  • 1395 Views
  • 2 replies
  • 0 kudos

CubeMX SD card initialization bug

In the update to CubeMX version 6.17, the SD card initialization (in my case, SDMMC2) was changed, and the software goes into "Error_Handler()". In my project I use STM32H7B0VBT6, FATFS, not RTOS.Specifically, version 6.17:static void MX_SDMMC2_SD_In...

cb.7 by Associate III
  • 344 Views
  • 6 replies
  • 0 kudos

CubeMX Bugs

Version 6.16.1I have identified a number of bugs - collecting them here.  Note that these are time wasters, but there are workarounds - so they are not critical but would definitely aid in the usability/productivity of users.-If you use the XCube.AI ...

Resolved! STM32WL5MOC Wrong LSE Drive Config in Example

I used CubeMX to generate the "LoRaWAN_AT_Slave" example for the B-WL5M-SUBG1 board.I had some issues with it waking up from sleep and upon a few hours of debugging i found that the LSE Driver Config was set to LOW in the example application, but the...

SKäli.1 by Associate
  • 219 Views
  • 2 replies
  • 1 kudos

Resolved! H5 Series filter doesn't work in MCU Finder

Since there is no caregory to post for the MCU Finder tool I'm posting here. On Windows, the stand-alone app, as well as the Android app, do not show any content when filtering by the H5 range in the series field. Could this please be fixed? It's bee...

etheory by Senior II
  • 201 Views
  • 1 replies
  • 2 kudos