2025-05-05 8:21 AM
I would like to report a bug, I post it here as so anybody can read it.
The bug concerns the GPDMA on STM32H563, but maybe it could happen on others MCUs. I wanted to use a GPDMA1 Channel from a ADC2 request, my Channel was correctly initialized, but the transfer between the ADC->DR and my buffer wasn't realized. I initialized correctly the Channel, with the correct Source and Destination addresses, in Circular Mode, from Peripheral To Memory, in Half Word size on the two sides, with destination address increment... I checked all of my configuration.
Until I checked the registers themselves... The REQSEL bits in the CxTR2 register of GPDMAx weren't initiliazed, they were equal to 0 instead of 1. These bits indiquates on which hardware request the transfer is done, something we configure in STM32CubeMX and should have been done correctly at the code generation... I added so this call in the ADC configuration function :
LL_DMA_SetBlkHWRequest(GPDMA1, LL_DMA_CHANNEL_1, LL_GPDMA1_REQUEST_ADC2); //Set Channel 1 hardware request to ADC2After adding this, it worked.
Solved! Go to Solution.
2025-06-16 6:51 AM
Hello @Karakala ,
Further to RM0481, section 16.3.5 GPDMA block requests.
You can find peripherals that works with GPDMA1/2 request as a block request.
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-05-06 2:55 AM
Hello @Karakala ,
First let me thank you for posting and welcome to the ST Community.
For more investigation, I suggest that you provide your Ioc.File.
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-05-06 3:02 AM - edited 2025-05-06 3:03 AM
2025-06-10 1:29 AM
Hello @Karakala ,
Sorry for the late reply. I am actually working on your request.
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-06-16 6:51 AM
Hello @Karakala ,
Further to RM0481, section 16.3.5 GPDMA block requests.
You can find peripherals that works with GPDMA1/2 request as a block request.
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.