User Activity

Hi all,some time ago I successfully developed a firmware for a ZigBee sleepy end device running on a STM32WB5MMG module. I could manage the module to draw only about 3µA in low power mode while still being able to communicate a button press over the ...
I have successfully implemented a ZigBee coordinator/router with an on/off-server-cluster based on a STM32WB5MMG module.My application is able to form a network and automatically allows certain off-the-shelf ZigBee On/Off-Clients to join the network ...
Hi All,Background: during my very first experiments with the STM32 Motor Control SDK 5.Y.2 I did hear something like a two tone alarm coming from the motor when a critical overcurrent or overload situation occured. I was pretty sure at that time, the...
Hi all,I try to implement a ZigBee device that acts as a Touchlink Target.My hardware is a STM32WB5MMG module. My debug UART is the LPUART1, no other UART configured.I use the STM32CubeMX 6.6.1 to generate the project and STM32CubeIDE 1.10.1 to compi...
Hi All,I am quite a newby regarding ZigBee since I have been playing around with this since bare a month now. So please be patient if my question might sound stupid or my terminology is not quite "ZigBee-conform".Short form of my question: Why do non...
Kudos from
Kudos given to