2025-06-19 4:05 AM
Hi! I have a STM32N6 discovery board and I want to create an application with network support for it. Lets say simple tcp echo server.
Ifound that there are no LwIP available for this board in CubeMX. Google suggests using Arure RTOS, but there are no such (X-CUBE-AZRTOS-N6) package. Instead, there are some "THREADX" and "NETXDUO" middlewares in configurator, but there are missing options to select PHY chip that is used on the board.
Is it possible to build network application using CubeMX on N6?