STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1549 Views
  • 0 replies
  • 2 kudos

Resolved! H5 Series filter doesn't work in MCU Finder

Since there is no caregory to post for the MCU Finder tool I'm posting here. On Windows, the stand-alone app, as well as the Android app, do not show any content when filtering by the H5 range in the series field. Could this please be fixed? It's bee...

etheory by Senior II
  • 204 Views
  • 1 replies
  • 2 kudos

Resolved! STM32CubeMX 6.16.0 – Fixed Nominal CAN Bit Timing Values

Hello,I’ve noticed a difference in behavior between STM32CubeMX configurations for STM32H7 and STM32N6 series.On STM32H7, when configuring CAN bit timing, the parameters such as Nominal Time Quantum, Nominal Time for one bit, and Nominal Baud Rate up...

Duc_0-1770995533811.png
Duc by Senior
  • 473 Views
  • 5 replies
  • 2 kudos

Using SPI DMA at 16bit, dosent work on STM32H5

Hi. ST There is an error in the code that is generated by CubeMx when you use 16bit in SPI DMA transfer. Can be solved in the stm32h5xx_hal_msp.c file: /* USER CODE BEGIN SPI4_MspInit 1 */ memcpy(&handle_GPDMA1_Channel1.Init,&NodeConfig.Init, sizeof(...

spa23 by Associate III
  • 2071 Views
  • 4 replies
  • 2 kudos