STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1626 Views
  • 0 replies
  • 2 kudos

Resolved! Uncluttering the Repository

My MX Repository has grown to more than 40 GB which is not exactly fun on the SSD of my MacBook. So I was wondering what made it so big.There seem to be all the zip files of all installed firmware packages. Does CubeMX/CubeIDE ever use them again?And...

Resolved! STM32H5 CubeMX HMI BSP Related Bug

It seems STM32CubeMX has a bug related to the STM32H5's HMI BSP component. If you do not wish to use this BSP component and want to configure the affected pins manually (like with other boards that do not have this HMI BSP component), the project wil...

No src folder created and code generation failed.

Hi everybody,I installed the last version of STM32Cube IDE (1.2.0) on two different computers, one is win7 an dthe second one is win10. When i strictly follow the tutorial to create a working project, I can see in both situations that the src folder ...

papageno by Associate III
  • 5185 Views
  • 5 replies
  • 1 kudos

Resolved! Potential bug in CubeMX for H733VGT6 with OCTO SPI?

Hi,I am trying to configure multiplexed OCTO SPI for the above MCU.Only Chip Select Port 1 NCS comes up as an alterantive for OCTOSPI1, and for OCTOSPI2 the Chip Select Port is is disabled, I would have expected Port 2 NCS to come up here... Is this ...

Southbranch_0-1706096065345.png Southbranch_1-1706096194909.png

Resolved! STM32 - FDCAN Interrupt not working

Hello,i'm trying to set up a new project with CAN in Interrupt mode. Therefor i generate a project with stm32cubemx and enabled the interrupt 0 for fdcan1 and also in the NVIC-settings the Interrupt is enabled:In polling mode, i can receive Frames an...

0693W00000AN0JsQAL.png 0693W00000AN0JxQAL.png
CSeif.1 by Associate II
  • 9445 Views
  • 6 replies
  • 0 kudos

STM32H7 Ethernet using FW V1.10.0 problems with memory?

I am adding ethernet connectivity to an existing STM32H743 project and am using the STM32CubeIDE V1.9.0 / STM32CubeMX V6.5.0 and H7 firmware FW V1.10.0. I have followed the guides on setting up the various memory settings and have had success gettin...

PMais.1 by Associate
  • 1843 Views
  • 1 replies
  • 1 kudos

CubeMX DSP BUG

在使用CubeMX生成Makefile工程文件时,在Mid中间件选项中选择“X-CUBE_ALGOBUILD”选项,并添加DSP Library,但是在最后的生成的项目文件中并没哟dsp.lib文件,应该是一个bug,望修复

ALO9611 by Associate II
  • 3549 Views
  • 6 replies
  • 0 kudos

STM32CubeMX: how to disable project saving on code generation?

Hello,I use STM32CubeMX in a shared project and different developers use different tools to work with its output. So e. g. I want code generation with a makefile output while others use the STM32CubeIDE.Currently every time when I click "generate cod...

jjwk by Associate
  • 3024 Views
  • 4 replies
  • 2 kudos