STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1547 Views
  • 0 replies
  • 2 kudos

STM32U5 ADF in LPBAM Mode

I want to use STM32U5 ADF in LPBAM Mode, I can't see the ADF option in the CUBE MX LPBAM design configuration. I want to use ADF in stop 2 mode with LPDMA and SRAM4 I have the ready code for ADF and LPDMA I wish to operate them in LPBAM Mode. 

SShai.3 by Associate II
  • 3833 Views
  • 6 replies
  • 0 kudos

Resolved! STM32H723ZG DMA I2S - tx works, no RX

HelloI've seen tons of posts about this, I'm hoping I'm just missing something simple, I would really love to get this working. STM32H723ZG, DMA TX works, I can send a sine wave fine but the RX buffer never changes and is never filled. I've put the R...

FDCAN: fdcan_tq_ck < fdcan_pclk requirement

We are using custom board with STM32H735. We were debugging the same issue as this one. In the reference manual RM0468, we discovered this note:I think this means that even when not using calibration unit, FDCAN kernel clock must be <= than APB1 peri...

heveskar_0-1706011696642.png

Resolved! STM32CubeMX-6.1.2 bug of generating SysTick clock source code

Hi, engineers of ST company. I want to consult you a problem about generating code for 'SysTick clock source'.Let us look at the first picture from documentation PM0215  page 63, there introduces the function of 'SysTick control and status register',...

hexiaole_0-1705920142853.png hexiaole_1-1705920190810.png hexiaole_3-1705921366220.png hexiaole_2-1705921342981.png
hexiaole by Associate II
  • 4550 Views
  • 5 replies
  • 3 kudos

Updating FreeRTOS to new version.

I use with CubeMx to generate FreeRTOS in stm32hf, and i would like to upgrade to version newer than FreeRTOS 10.3.1 (because security issues in this version) so, i took manually the newer FreeRTOS files(10.5.1) and replaced them instead what that Cu...

dToub.1 by Associate
  • 3496 Views
  • 1 replies
  • 0 kudos

STM32CubeMX creates a lot of garbage in user home directory

Hello community,I use STM32CubeMX 6.10.0 in Ubuntu 23.10.Each time I start a session, I noticed that about 65 MBytes of data are used in ~/.stm32cubemx/.jxbrowser-7.35.1/Profile/xxxx which are never deleted when I exit.A new profile subfolder is crea...

Oskar_H by Senior
  • 3937 Views
  • 4 replies
  • 4 kudos

User Authentication : why ??

Hello community,I have just installed the latest release 6.10.0 of STM32CubeMX on latest Ubuntu 23.10 and tried to play a little with it.Previously I was using a very old release in my projects and uninstalled it quite a long time ago for many reason...

STM32CubeMX_ApplicationsList.png STM32CubeMX_ApplicationsMenubar.png STM32CubeMX_UserAuthentication_Cookies.png STM32CubeMX_UserAuthentication_Scrollbar.png
Oskar_H by Senior
  • 8899 Views
  • 9 replies
  • 18 kudos

Resolved! USART Configuration

Hi,I need help configuring a USART connection between a STM32L452RE Nucleo Board and a ESP8266-01 wifi chip. My goal is to send AT Commands from the STM32 to the ESP8266.I currently have my USART TX and RX connected to the RX and TX respectively of m...

wifi commands.jpg com.jpg usart.jpg
khaylup by Associate
  • 4613 Views
  • 4 replies
  • 5 kudos

How to get more boards on STMcubeMX?

Hi all, Currently I am trying to program the STEVAL-MKI109V3 carrying the STEVAL-MKI227KA sensor board via the STM32cubeMX and IDE platforms. However the STEVAL-MKI109V3 board is not available on the STM32cubeMX software. Are there any expansion pack...

ZoeTakacs by Associate II
  • 1072 Views
  • 1 replies
  • 0 kudos

STM32H733: USB HAL initialization ends up in Error_Handler()

I'm using STM32H733VGT6, USB configured as: External Phy: Device_Only,Speed: Device Full Speed 12 Mbit/s, USB tacting from HSI48 And initialization ends up in Error_Handler(), anyway.. All is up-to-date, updated today, software packages, etc, STM32Cu...

Bacamhao by Associate
  • 2378 Views
  • 3 replies
  • 2 kudos