cancel
Showing results for 
Search instead for 
Did you mean: 

Hi! I am trying to install the STM32CubeMX 6.8.0 on my macOS 13.3 (Ventura),when I run the installer it gives me the following error: You cannot open the application SetupSTM32CubeMX-6.8.0.app because it is corrupted or incomplete.

CColo.2
Associate III

I have installed Xcode and tried to run the instructions "In case of error, try one of the following fixes: - $sudo xattr -cr ~/SetupSTM32CubeMX-6.8.0.app."

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Ghofrane GSOURI
ST Employee

Hello @CColo.2​ 

First let me thank you for posting .

Let's try to uninstall and reinstall CubeMX again .

This is the LINK to download the Latest version CubeMX 6.8.0

Uninstalling STM32CubeMX on macOS® :

There are two different ways to uninstall STM32CubeMX on Mac:

1. Move STM32CubeMX.VERSION.app to the trash

2. Use the following command line:

a) For STM32CubeMX 6.2.x and later versions only: cd SetupSTM32CubeMX-VERSION.app/Contents/Resources/Uninstaller ./uninstall.s

To install CubeMX 6.8.0 On macOS please follow those steps :

a) On STM32CubeMX-Mac line, Click “Get software�? to download the package 

b) Extract (unzip) the downloaded package.

c) Make sure you have administrator rights. 

d) Double-click SetupSTM32CubeMX-VERSION.app application file to launch the 

installation wizard.

In case of error, try to fix it: - $sudo xattr -cr <Folder where the zip was extracted>

Thx

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

CColo.2
Associate III

Hello Ghofrane GSOURI,

Thank you, the problem I had was the Beta version of macOs Ventura 13.3, it wouldn't let me install the software, I reinstalled the normal Ventura 13.3 version, I installed the CubeMX 6.8.0 version without a problem and then I updated to the Beta version of the macOS.