cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX directory structure not shown on MAC OS for certain folders

ABucs
Associate II

A very strange things happened when trying to browse (open a project) on most of the directories located on my MAC (OS Monterey on Apple M1 MAX):

  • I cannot see the folders structure when accessing Documents
  • I can see folders when accessing Pictures

The directories informations looks identical (see the pictures)

Can you please explain what is the reason? I use the latest STM32CubeMX.

Thanks,

Andrei

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
timistof
Associate III

What worked for me is to add STM32 Cube MX to list of the apps that get allowed "full disk access" under System Preferences -> Privicay & Security -> Full Disk Access.

View solution in original post

4 REPLIES 4
MJ042
Associate II

Hi @Community member​ , have you been able to solve this issue? I'm facing the same issue.

snigg
Associate III

Any updates here. I have the same issue and believe it could be connected to security features of OS X and bad programming from ST side... The tool almost unusable since I can not load old files. On one installation of OS X (Monterey) I can't even store the file-settings.

timistof
Associate III

What worked for me is to add STM32 Cube MX to list of the apps that get allowed "full disk access" under System Preferences -> Privicay & Security -> Full Disk Access.

ABucs
Associate II

Ye this solve the problem. I'm not sure how safe it is as CubMX can erase with no asking an entire directory...

But works!