STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1589 Views
  • 0 replies
  • 2 kudos

STM32U5 IAP_main example NOT working

Hi,I am using STM32CubeMX version 6.11.0 .I want to test the "IAP_main" example for the STM32U575I-EV.I start the project as follows : Then when I try to Generate Code for the STM32CubeIDE in CubeMX the following error occurs: The code gets generated...

IAP_main_u5_error0.png IAP_main_u5_error1.png IAP_main_u5_error2.png

Resolved! STM32U585QII6Q ADC4 Channels

Hello,I'm encountering an issue with STM32CubeMX while configuring the STM32U585QII6Q microcontroller. Specifically, when attempting to configure PD11 to ADC4_IN15, I find that the ADC4 channels are grayed out or inactive.While using STM32CubeMX, I c...

ari_v2 by Senior
  • 1887 Views
  • 2 replies
  • 0 kudos

Resolved! NUCLEO-H563ZI SPI Master example is not working

Hi I'm trying to run SPI_FullDuplex_ComIT_Master and Slave examples that use SPI1 on NUCLEO-H563ZI boards.The pin connections in the read me seems to be inaccurate i.e1. There is no PA5 on 10th pin of CN6 on the Nucleo but it is there on CN7.2. There...

WCarey_0-1712129354068.png
WCarey by Associate III
  • 2164 Views
  • 4 replies
  • 0 kudos

Resolved! STM32H750B-DK setup the BSP folder through the .ioc file

Hi,I am following a course (for a different STM board) to use the LCD touchscreen of the STM32H750B-DK board. In the course, they have added a BSP folder to their project which includes files such as are seen here: STMicroelectronics/stm32h750b-dk-bs...

Bxy by Associate II
  • 2601 Views
  • 2 replies
  • 0 kudos

Resolved! CUBE MX with Keil 5.39 Full Assert bug in stm32l0xx DFP

Encountered an annoying project generation bug recently. By default CubeMX adds to keil project a hwhole bunch of files:Even if you don't need any of the LL. So, when you tick "Enable Full Assert" checkbox, it causes an error, because no "stm32_asser...

MaxFlatline_1-1707994561233.png MaxFlatline_0-1707994799324.png MaxFlatline_1-1707994814780.png