User Activity

Hello, I have a design with an STM32F446RCT6 where I use the FatFS file system and the USB HS as USB Host in Mass Storage Host Class.The design is made with STM32CubeIDE 1.8.0 and the firmware package is V1.26.2 / 16-july-2021.The configuration param...
Hi, I have an unsolved issue with SDcard.The project is based on STM32L476, the IDE is Atollic and configuration is made by STM32CucbeMX (as I do with all my designs).Without DMA (no DMA template in FATFS and no configured DMA channels) the SDcard wo...
Hello, I am trying to start the bootloader on a STM32F427 to program the MCU via USB port in DFU mode. I am not new to this topic because I wrote some programs for STM32F072 where I can successfully start the bootloader and take externally control of...
I am using a STM32072B-EVAL board because I need a working demo about HDMI-CEC.It is clear that there are problems: the original firmware already on the board has errors about icons (some graphics is broken), about images (it hangs if try to show an ...
Posted on March 31, 2014 at 15:44Hello, I have a problem similar to the one discussed in the post named ''STM32F103RB - Different Clock Speed Between Reset?''https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=ht...