User Activity

I am using the following setup:- STMCubeIDE1.6.1 on Windows 11I see the following behavior- Opening the IDE with the default Toolchain and my Project for 1.6.1 works fine and build. However, I need to use the GNU Tools for STM32 (7-2018-q2-update)- I...
I am using the STMH7A3ZI-Q Nucleo Board together with the WFM200S Silicon Labs WiFi Board.The example project of the WFM200S uses the deprecated SDIO library with an F4 Nucelo ( (https://github.com/SiliconLabs/wfx-fullMAC-tools/tree/wifi_examples_ssv...
I am trying to connect to the WFM200 wifi module over SDIO. I am using the SDMM peripheral library/code for this.However, in the selection in CubeMX there is only the options for SD and MMC but no SDIO.Which option should I choose for using SDIO with...
Hi,I cannot find any information about the possibility to use github copilot in the STM32CubeIDE. Is it available or are there any plans to support it in the future?Or do you recommend using it in VS only?Thanks you for your answer
I am working on an existing project based on the STM32H750 where I want to stop overheating by reducing the CPU frequency.Currently I use 400MHz and I want to lower it to 200MHz. I have peripherals (LCD and SPI flash) as well as timers (TIM1,2,5) tha...
Kudos from
Kudos given to