STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1592 Views
  • 0 replies
  • 2 kudos

STM32CubeMX 6.13.0 released

We are pleased to announce to you that the release 6.13.0 of STM32CubeMX is available. What is new in 6.13.0: Added support for the following series, microcontrollers and microprocessors: STM32N6, STM32U3, STM32WL3x, STM32G411xx and STM32C0Added the ...

Resolved! STM32CubeMX Release 6.3.0 crached after start

I have the following big problem:I had installed previously release 6.2.0 of STM32CubeMX and everything works fine. Then i uninstall this release and update to the new one 6.3.0.Now the programm craches after start. An backgroundprocess at windows fo...

TLoew.1 by Associate
  • 2076 Views
  • 3 replies
  • 0 kudos

CubeMx: selecting Firmware Path

Why can't I change the Firmware Relative Path when I have unchecked the "Use Default Firmware Location"?I clicked the "Browse" button and there was no response.

Ryan71 by Associate II
  • 3890 Views
  • 7 replies
  • 1 kudos

Resolved! Automatic USART Baudrate detection for STM32H523

Hi, I have tried to configure the STM32H523RET6 for using USART1 with multiprocessor communication mode and enabled the auto baudrate detection. However, according to the application Note AN4908, the MCU stm32h523 doesn't support auto-baudrate. I don...

hakeila by Associate III
  • 1319 Views
  • 1 replies
  • 1 kudos

Resolved! OCTOSPI and MDMA - STM32CubeMX bug

Hello!I would like to report a bug. Using STM32CubeIDE 1.16.0 and the integrated STM32CubeMX 6.12.0 i encountered a bug regarding OCTOSPI and MDMA on STM32H723ZGT6 MCU. Inside HAL_SPI_Receive_DMA(handle, pdata); where the HAL_MDMA_Start_IT is called ...

samob2703_0-1722426480442.png
samob2703 by Associate II
  • 1787 Views
  • 2 replies
  • 2 kudos