User Activity

Hi,I would like to create a project with CubeMX where I handle files on a SD card with FAT Fs file system using a STM32U5 mcu.When I select the STM32U5 MCU in CubeMX  the FATFS middleware is not available, while If I select other MCUs series like STM...
Hi,I am using STM32CubeMX version 6.11.0 .I want to test the "IAP_main" example for the STM32U575I-EV.I start the project as follows : Then when I try to Generate Code for the STM32CubeIDE in CubeMX the following error occurs: The code gets generated...
Hi,I want to migrate a project that I have made on a STM32L4 where I make the spectral analysis of the noise that I read from a digital MEMS microphone using the arm_fft dsp functions to a new board with a STM32U5 mcu.I have tried to include the "lib...
Hi,I am testing the Soundmeter Example provided in STM32CubeMX for the NUCLEO-F401RE board in conjunction with the expansion board NUCLEO-IKS02A1.The example works, but the results I get in the Unicleo GUI are not the expected ones.I am testing the b...
Kudos from
Kudos given to