STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

customized keyboard using stm32 f44 series controller

Hello everyone,as I am developing keyboard with extra keys adding to the existing key board. I am adding extra modifier keys to the key board to perform the task. kindly let me know will it work and give suggestion inputs. my customized keyboard cons...

SSRIN.2 by Associate III
  • 4135 Views
  • 7 replies
  • 4 kudos

Resolved! How to get the value of the program counter ?

Hello, Sometimes I have my stm32F7 going in hardfault_handler, so for my customers I have to display on a screen the last address where the software crashed, then I can analyse which problem occure the crash. So I want to get the value "pc" (program ...

PierreG-S by Associate II
  • 4141 Views
  • 2 replies
  • 2 kudos

Resolved! STM32u585 Memory Mapped Read/write on B-U585I-IOT02A

While using memory mapped mode for APS6408L using STM32u585 on B-U585I-IOT02A, how is the row boundary crossing handled?* If I want to write across multiple Rows in memory mapped mode, do I need to handle this manually or is it automatically handled ...

Bootloader v11 + changes

I've been using an STM32G474xx in a project for a few years now and have a function that jumps to the bootloader. It seems in a recent rev of the chip the bootloader has changed. I'm finding that I can no longer jump to the bootloader similar to how ...

PCarn.1 by Associate III
  • 1702 Views
  • 2 replies
  • 0 kudos

Failure when migrating STM32CubeMX project to compatible part

I have tried to migrate an STM32CubeMX project from the STM32H747AIIx to the STM32H747XIHx using the procedure described here:How to switch from one STM32 to another using STM3... - STMicroelectronics CommunityIt failed with the following error messa...

ACaru.1 by Associate II
  • 1667 Views
  • 2 replies
  • 0 kudos

Resolved! Debouncing

Can anyone help me with debounce code in C for Rising and falling edge interrupt??

sne_123 by Associate III
  • 26301 Views
  • 20 replies
  • 4 kudos

STM32H723 - Problem with Serial RAM in memory mapped mode

Hi everyone,I’m testing a 32Mb serial QUAD SPI RAM (ISSI – ISS66WVS4M8) with the nucleo – H723ZG development board.It works fine if I use all the QUAD SPI commands but my need is to use it in memory mapped mode.When i use the memory mapped mode confi...

MDell.1 by Associate II
  • 17544 Views
  • 14 replies
  • 3 kudos

MDMA write error writing to DMA registers

Hello, I have a DMA stream working in Normal mode (Mem to Peripheral). This by itself is working properly (without MDMA). I want to configure MDMA to set the next parameters for the DMA to handle. I configure 4 words (4 uint_32) in memory for writing...

BBeha by Associate II
  • 889 Views
  • 0 replies
  • 0 kudos

STM32l496: Clocking timer using LSCO

Hi, I wanted to clock my timer output using LSE crystal, but unfortunately only tim2 is supported with this feature. But then I saw an option of LSCO as output in cubemx, this enables the pin on MCU and according to documentation this output LSE cloc...

HZaib.1 by Associate III
  • 2998 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.