STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

peripherals power consumption of stm32u585 in stop mode

Hello, In the MCU datasheet, there is a table on page 200: Table 72. Typical dynamic current consumption of peripherals.What is the meaning of the current writing in the peripherals on stop modes, since in this mode, all clocks in the core domain are...

amit3 by Associate
  • 437 Views
  • 1 replies
  • 0 kudos

Resolved! HAL_ADC_Start_DMA caused main loop to become blocked?

Hi, I am configuring the ADC in single-channel continuous conversion mode using DMA. However, once I call HAL_ADC_Start_DMA(&hadc, &AD_RES, 1), the main loop stops executing, and the HAL_ADC_ConvCpltCallback() function is not triggered.I noticed that...

Resolved! OCTOSPI signal integrity issue on STM32H723 vs STM32H725

Hello everyone,This is my first post on the ST Community forum.I recently moved from a custom 6-layer board using STM32H725IGKB to a simpler 4-layer board using STM32H723ZGT6. Both designs use an external OCTOSPI memory, with 50 ohm controlled-impeda...

Jonshill by Associate II
  • 491 Views
  • 3 replies
  • 0 kudos

Resolved! Minimum hardware requirements for STM32F765

Can anyone tell me or direct me to a source that shows the minimum connections needed to power up and serially program a STM32F765ZGT6? (144 pin package.) I will be attaching the chip to a breakout board and will be using a St-Link Minie3.  Any help ...

Resolved! USBPD EPR Request

Hi! I'm working on a Power Delivery Sink using an STM32G484RETx MCU. I managed to get SPR Power Delivery working without any issues, but I'm having trouble handling the EPR handshake.I'm using the latest USB-PD library from ST's GitHub:https://github...

epr.jpg epr2.jpg
KamilB by Associate II
  • 1297 Views
  • 7 replies
  • 0 kudos

Resolved! OCTO SPI output impedance on H7-series

I have swapped from a custom PCB-board with a 6-layer stack using a STM32H725IGKB, to another custom board with a 4-layer stack using STM32H723ZGT6 (simpler package).I am using an external OCTO SPI on both boards, but I have R/W errors with the 4-lay...

PWM to ADC synchronization unexpected delay

Hello everybody,I am trying to synchronize the ADC1 and ADC2 to work with center-aligned PWM signals in dual-simultaneous regular mode using DMA. My setup:PWM frequency: 5.2 kHZADC conversion frequency: 104/2 = 52 MHZIf I have 3 conversions per ADC w...

richi_0-1766693549208.png richi_1-1766694295760.jpeg richi_2-1766694449913.png richi_3-1766694470632.png
richi by Associate III
  • 1017 Views
  • 5 replies
  • 0 kudos

STM32U575 Bank1 Flashing Problem from Bank2

I am trying to do OTA programming modifications using the DUAL bank feature of my STM32U575 IC with 1Mbyte of memory.I have successfully done this when the program starts in BANK 1 and I reflash BANK 2. I change the User Option byte to OB_SWAP_BANK_E...

Resolved! Strange behavior of STM32G070RBT6 ADC

I am facing very weird issue in STM32 ADC.1. I used single channel in polling mode and interrupt mode the value i got was 4095, even the pin voltage was 1.7V, i used DSO to look for any serious noise on the pin but it was clean.Also if i gave 0V to t...

psain.1 by Associate III
  • 662 Views
  • 3 replies
  • 3 kudos