STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H562IIT6- XIP support

For the microcontroller STM32H562IIT6, does it support code execution from External flash(Xip)? Also does it support Quadspi interfacing in given Octospi lines?

APras.2 by Associate II
  • 240 Views
  • 1 replies
  • 0 kudos

STM32G031Y8Y6TR ultrasonic cleaning

Can the STM32G031Y8Y6TR be subjected to ultrasonic cleaning after being mounted on the board? Are there any internal structures that do not allow ultrasonic cleaning?1. **Cleaning agents**: ST-240KKA or pure water2. **Temperature**: 55°C or below3.**...

Xiangkui by Associate
  • 189 Views
  • 1 replies
  • 0 kudos

STM32N6 VENC Hardware Handshake with MJPEG encoding

The VENC peripheral on the N6 boasts a hardware handshake path with the DCMIPP peripheral, potentially allowing full compression of each frame to occur with very little active RAM. From what I can find, the DCMIPP capture starts, then the VENC is tol...

chornbeck by Associate II
  • 1046 Views
  • 4 replies
  • 3 kudos