STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

OSC32 - use pc14/15 as GPIO

Posted on February 08, 2012 at 16:02Hi, How can i use PC14/15 as GPIOs? I turened off  LSE by using this function and configure PC14/15 as input floating:      RCC_LSEConfig(RCC_LSE_OFF);  But  the ports does not read any data, What do i miss?

ybitton by Associate II
  • 1286 Views
  • 1 replies
  • 0 kudos

PDM audio software decoding library?

Posted on January 18, 2012 at 17:17 Here is a description of the PDM audio software decoding library from the AN3998 PDF: The PDM audio software decoding library includes one header file pdm_filter.h and binary/object codes for the following ...

ozvena by Associate II
  • 2287 Views
  • 4 replies
  • 0 kudos

Timer slave mode : Reset mode

Posted on February 09, 2012 at 11:51 Hello, I would like to use a timer on Reset mode, but I have some problem : My goal is to never call the timerinterrupt until the trigger input is switching. I want to enter in the timer inte...

Power consumption ?I

Posted on February 08, 2012 at 03:43Hi, Currently, I am designing an application board for STM32VLdiscovery with batteries. In order to decide the parameters of step-up converter, I would like to know the current consumption of STM32VLDiscovery, alt...

takita by Associate
  • 746 Views
  • 1 replies
  • 0 kudos

STM32F4 max speed with FSMC

Posted on February 08, 2012 at 20:30I am new to arm and designing a new prototype board with a STM32F417 and 2 NAND Flash chips. In the data sheet it says the HCLK can go to 168MHz BUT it also says that the FSMC maximum clock is 60MHz at 3.3V.  Does...

kb by Associate II
  • 1546 Views
  • 1 replies
  • 0 kudos

External 16550 with STM32F103 FSMC

Posted on February 08, 2012 at 20:49I have an application that needs 9 (yes, 9) serial ports.  The STM32F103 I am using supports 5, so I am adding an external 16554 quad uart.  As part of my testing before actually getting a board built, I am trying...

jwormsley by Associate III
  • 762 Views
  • 0 replies
  • 0 kudos

STM32 SPI port

Posted on February 06, 2012 at 18:02I am trying to interface with an SPI port device which requires a 24bit transfer, I have successfully managed to achieve this using the example code and standard peripheral library but I am seeing gaps between byt...

dwooller by Associate II
  • 2194 Views
  • 6 replies
  • 0 kudos

Data initialization in flash memory on stm32f103 controllers

Posted on February 07, 2012 at 07:36  Hello! I'm looking for information - how to initialize data (e.g. arrays, strucutures etc.) in flash memory. It isn't enough RAM memory for my programm.  I'm using Atollic TrueSTUDIO®/STM32 Lite IDE. I think th...

nazmievr by Associate
  • 1275 Views
  • 2 replies
  • 0 kudos