cancel
Showing results for 
Search instead for 
Did you mean: 

RTOS demo for STM32L-Discovery

disirio2
Senior
Posted on October 04, 2011 at 18:27

Hi,

Starting from version 2.3.3 ChibiOS/RT includes full support for the STM32L and a full demo for the STM32L-Discovery board.

The demo guide is available here:

http://www.chibios.org/dokuwiki/doku.php?id=chibios:articles:stm32l_discovery

The application demonstrates the use of the following components:
  • Cortex-M3 startup support.

  • Linker scripts for STM32L.

  • STM32L-Discovery specific board files.

  • RTOS kernel for multi-threading and synchronization.

  • HAL driver for the STM32L platform initialization (clock tree).

  • PAL driver (I/O ports abstraction).

  • DMA driver (shared DMA abstractor helper driver).

  • ADC driver in DMA mode.

  • SPI driver in DMA mode.

  • PWM driver.

  • Interrupt driven serial driver.

  • Test Suite for self test and reporting.

Similar demos are also available for the STM8S-Discovery, STM8L-Discovery and STM32VL-Discovery. STM32F4-Discovery support will be introduced next.

Giovanni

---

http://www.chibios.org

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0