Skip to main content
kermespersialainen
Associate
October 6, 2011
Question

Huge STM32 Flash Loader Demonstrator 2.4.0 issue

  • October 6, 2011
  • 1 reply
  • 746 views
Posted on October 06, 2011 at 07:56

Hello everyone,

I just received a STM32100E-EVAL board and wanted to download software to it with freshly installed STM32 Flash Loader Demonstrator version 2.4.0. Previously I had some 2.x version but wanted to upgrade in case it did not support the STM32F100ZE chip. The 2.4.0 version did get a response from the F100ZE chip, but shows red traffic lights and the only button to push there is the remove protection button, which does not work.

I first thought it is a problem with the F100ZE, but I cannot continue from there. The 2.4.0 loader does not work with any other board we have, with different STM32 microcontrollers, I cannot see anything else than red traffic lights.

I have tried this on two different Vista laptops, with and with two different USB to RS232 serial adapters.

It does seem that on a third laptop that has a real RS232 serial port and running the Flash Loader 2.2.0 can program the F100ZE on Win XP.

So, any suggestions? Is this a known bug? Can I download older versions that *do* work?
    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    October 6, 2011
    Posted on October 06, 2011 at 17:02

    Can I download older versions that *do* work?

    I posted them up here before, because ST doesn't have an FTP site that you could get old versions from, but I think the forum ate them in the May 2011 crash.

    I have um0462 versions 1.2 circa Nov 2008, 2.0 Jul 2009, and 2.1 Nov 2009, which should be attachable here. If that fails, specific requests can be set to me at sourcer32@gmail.com provided you have an email account that is capable of receiving 8MB ZIP files

    ________________

    Attachments :

    um0462_1_2_nov_2008.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtSv&d=%2Fa%2F0X0000000aQM%2Fb.pm9mcX3JyDkCDWysrze_mGA4zW79UJba_F9MkI8n8&asPdf=false

    um0462_2_0_jul_2009.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtUl&d=%2Fa%2F0X0000000aQo%2FmJ1GO7obnPlJvPDMjzNln.oe5bk7mVKw1Ci60PVTh68&asPdf=false

    um0462_2_1_nov_2009.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtUq&d=%2Fa%2F0X0000000aQq%2FxeMXJtqtNWgbCqwXM1V3R82uYYLFvbSaa0GyNM1ddbg&asPdf=false
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..