STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

delay from two signals

Posted on April 03, 2012 at 20:12Hello at all, I have to mesaure the delay between 2 signals that I have in input to the microcontroller. I saw the example of the PWM input. I supposed to use an OR gate to have both front to the same pin but I think...

momede by Associate II
  • 2499 Views
  • 5 replies
  • 0 kudos

ST32F217 with STE100P. How to configure PHY address?

Posted on April 04, 2012 at 07:04STE100P how to set PHY address?Hello. Im trying to using an STE100P PHY ethernet chip (with ST32F217 MCU). In the datasheet for STE100P i see an description for bits 7~3 PAD4:0 in PR20- XMC, XCVR Mode control registe...

andrey23 by Associate II
  • 2205 Views
  • 4 replies
  • 0 kudos

Ethernet PHY DP83848CVV

Posted on April 04, 2012 at 13:55Hello, I want to use DP83848CVV as Ethenet PHY with STM32F207ZET6 in RMII mode. In Schematics (STM3220G_EVAL),there is some resistor of 51 Ohm in between of  signals (RMII_REF_CLK,RMII_TX_EN,RMII_TX_D0,RMII_TX_D1,RMI...

migrating from Atollic to IAR

Posted on April 05, 2012 at 07:39Hello, reasently i changed ide to iar and i getting strange problems: i have working code developed in atollic and tested on my discovery boards, but then i use same code on IAR, it just doesn't work. Like touchscre...

linas2 by Associate II
  • 1604 Views
  • 3 replies
  • 0 kudos

STM32F207

Posted on April 04, 2012 at 12:16Hello, I would like to download a C compiler for STM32F207. Where I could find it? I was searching through the forum, but without success. #stm32f207 #c/c++-compiler

dove457 by Associate
  • 1410 Views
  • 2 replies
  • 0 kudos

RTC calibration

Posted on March 29, 2012 at 07:42Hi all,I wanted to know is there any software workaround to compensate for negative ppm values.I am using STM32F100V8 controller. According to the rtc digital calibration manual(attached) you can only subtract the cy...

Boring problems with ST LINK on STM32LVDISCOVER

Posted on April 04, 2012 at 17:17Hi folks,I have big problems with connecting to ST LINK integrated on ST discovery kit. I already install all utilities, driver updates (V2) and  test all tips and trick posted in forum, but the result is same...''Ca...

Register or Standard Peripheral Library

Posted on March 31, 2012 at 17:58Hello, I am new to this forum. Is there anyone who does not use Standard Peripheral Library for programin STM32F4 ? I'm don't like SPL and and programmed using registers for set the uC. I greet

we by Associate II
  • 1717 Views
  • 7 replies
  • 0 kudos

Backlight Driver STLD41 producing disturbance on TFT

Posted on April 04, 2012 at 14:08Hello I am using STLD41 as backlight driver for 5.7''controllerless TFT. Whenever STLD41 gets on it produces lines on TFT & display gets disturbed.If i give backlight power seperately from power supply Display works ...