Posted on May 17, 2011 at 13:35Hi, Help an overwhelmed STM newbie for Christmas! There is an old *** pre-CMSIS *** application implementing a DMA parallel port triggered off an external clock signal described in an2548.zip (in the old pre-cmsis firm...
Posted on May 17, 2011 at 13:35Hi, I sucseefully flash the firmware required for the B Eval Board to connect to the DFU PC application. I also see that when using the USART IAP toolt that the memory is not right protected, so everything should be ok...